0 to 50% Manual Outside Air Damper
When a 0 to 50% manual damper is installed, with any supply fan type, the outdoor air damper is
controlled to a setpoint from a Remote Minimum Position (wired input), Manual Damper Position
Setpoint, or Economizer Minimum Position Setpoint BAS.
Model Number: | Used With: |
FIADMPR102* | T/YS*072-150 |
FIADMPR103* | T/YS*180-300, W/D/GS*150-300 |
Introduction
Read this manual thoroughly before operating or servicing this unit. See the download link below.
Note: This accessory is not for use on units with Single Zone VAV or True VAV supply fan types (Digit 15 = 2,3,4,5).
Note:
How to configure the Symbio 700 for motorized damper accessory:
Settings > View Configuration > Edit > Stopping the Equipment (Proceed) > Outside Air
Change:
Outside Air - 0 to 50% Motorized Damper
Remote Minimum Position- Not Installed
Click the e-library symbol for the latest version
Click the e-library symbol for the latest version
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.