Power Exhaust - Symbio Precedent 6 to 25 Tons - Installation Guide for Standard and Low Leak Economizer
Summary:
Power exhaust is designed for downflow applications¹. If the installation is for horizontal duct connections, the power exhaust may be mounted on the horizontal return duct. The installer is responsible for the installation. An economizer or motorized damper must be installed and functional before attempting to install the power exhaust. The power exhaust can be turned ON at infinite fresh air damper settings depending on how the unit is configured.
(1 Downflow application only is possible for units with low leak economizers.)
Model Number: | Used With: |
FIAPWRX302* | T/YS*072-150*3 |
FIAPWRX402* | T/YS*072-150*4 |
FIAPWRXW02* | T/YS*072-150*W |
FIAPWRX303* | T/YS*180-300*3, W/D/GS*150-300*3 |
FIAPWRX403* | T/YS*180-300*4, W/D/GS*150-300*4 |
FIAPWRXW03* | T/YS*180-300*W, W/D/GS*150-300*W |
Introduction:
Read this manual thoroughly before operating or servicing the unit. Click the e-library image below to download the latest PDF of the Power Exhaust Guide.
Wiring Diagram for FIAPWRX*02*:
Wiring Diagram for FIAPWRX*03*:
Configuration:
From the Home screen < Settings < View Configuration < Edit < Proceed and Space Pressure Control to Relief Fan Only
Possible Alarms:
Relief Fan Output Status
Click the e-library symbol for the latest version
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.