Attached is the IOM and the Product Catalog which contains the Wiring diagram for the 0036/0048/0053 , also the sensor locations and Error codes associated with , these units can have multiple Indoor units , based on capacity .
4TVH0036/0048/0053 Mini Splits IOM/PROD Catalog
Articles in this section
- VRF LEGACY OUTDOOR AND WATER SOURCE IOM"S
- TUT SETUP/CONNECTION
- E154
- VRF E201 Emergency Operation
- Samsung Ductless Prospace Service Manual - Error Codes, Diagnostics, Wiring Diagrams
- VRF EEV Resistances
- Wired Remote Controller
- Wired Remote Controller/User Guide
- Emergency Temperature Output Function
- VRF PRODUCT OPTION CODES