Issue:
Is there a trick to installing the seal ring around the piston?
Resolution:
RTAA, RTWA, RTUA, RTHA, RTHB, RTHC, RTHD chillers:
- Slide the inside edge of the seal (compression) ring around part of the outside diameter of the piston
- Use a rounded object such as a large socket and roll it on the inside of the seal (compression) ring to slide over the outside diameter of the piston, similar to how a tire mounting machine fits a tire over the wheel
Notes:
Changes:
Other Question/Problem/Cause Statements:
- Is there a trick to installing the seal ring around the piston?
- Is there a trick to installing the compression ring around the piston?
- Is there a trick to installing the wear ring around the piston? (Not wear ring, but seal ring.)
- How do I install the compression ring on the piston?
- How do I install the seal ring on the piston?
Facts:
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Air-Cooled Chiller (Charmes) (RTAA)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
Document Identifier: DOC-74072
Document Identifier: 74072
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.