Summary:
This process outlines how to load a controller configuration onto a UC or Symbio controller using Tracer TU.
Resolution:
1. From the Utilities dropdown, select "File Transfer Utility."
2. Make sure the box is checked next to the controller’s name and click next.
3. Browse to and select the Config file and click Open.
4. Verify the correct file is in the window, click on Next, then click on Start.
5. When the update is completed, select Finish.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.