Error Code E0
Summary:
Power phase loss/reverse/under-voltage/over-voltage fault
Possible Cause:
- Power supply is incorrect (Lack of phase, phase stagger, under-voltage, over-voltage)
Troubleshooting:
- If the power supply is missing a phase (correct the lack of phase)
- If the phase sequence of the power supply is incorrect (Use a phase sequence meter to check the phase sequence of the power supply. This device can indicate whether the sequence is correct or incorrect.)
- Under-voltage or over-voltage (If the power input between L1 & L2 ≥ 260V or ≤ 180V(for 230V products)) / (If the power input between L1 & L2 ≥ 518V or ≤ 403V (for 460V products)) - Correct the supply voltage