- This is Usually seen when the Factory jumper is not installed back at CN31 On the Inverter board after it has been replaced.
- If the unit has two compressors it will connect to CN31 On the top Inverter #2 .
- If the unit only is a single compressor it will connect to the single inverter module at CN31.
- E205-U200 is the Main unit.
- E205-U201 is the first sub unit.
- E205-U202 is the second sub unit.
- These are determined by the Dip switches for Gen 1 and programmed in Gen 2 units.
- Gen 2
- Gen 1
-
- Trane Part number if lost or needs to be replaced .
WIR07708 5 1 WIRE; WIRE; ASSY, CONNECTOR-INVERTER SHORT, DVM I
E-205
Articles in this section
- VRF SC GATEWAY CONNECTION W/O SILVERLIGHT
- Trane Branded Samsung Water Source IOM
- Trane Branded Samsung Warranty Information
- Trane Branded Samsung cassette IOM'S /Catolog/Panel instructions
- Mode Control Unit (MCU
- VRF AUTO PORT PAIRING
- Air Handling Unit (AHU) Application Kit
- E320 Error Code for C-Series and Mini VRF units
- Outdoor Unit Operating Priority
- C-Series U Match , 4TUK,4MUD, 4MUC, 4MUW/ Trane Branded Samsung 1 To 1