The Trane Symbio 700 equipment controller pairs with the Symbio mobile application using Bluetooth Low Energy (BLE). When paired with the Symbio 700 controller, technicians can use the Symbio mobile application to edit operating setpoints, adjust other parameters and settings, and perform a range of service and troubleshooting tasks while standing at the unit.
Make sure you give the app full permissions; if not, the phone app won't connect with the Symbio Unit Controller.
Needed to connect to the Symbio 700 Bluetooth
-
Smart devices supported:
- iPhone®
- Android™
- Trane Symbio Service & Installation mobile app
Connecting to the Symbio 700 Controller
- Enable Bluetooth on your smart device.
- Access the Symbio 700 unit controller in the low-voltage section of the equipment.
- Press on the Symbio 700 keyboard/display to turn on Bluetooth.
-
Confirm the status of Bluetooth communications.
Blue LED Display DescriptionBlue LED Display Description Press for On/Off
Off NOT CONNECTED Bluetooth Off Blinking WAITING Bluetooth On — Not Paired On Solid CONNECTED Bluetooth On — Connected/Paired Symbio 700 Bluetooth status
- Start the mobile app on your smart device.
- On the login screen, press [View Available Devices] in the lower portion of the screen. Or Trane personnel can log in using their Trane Connect username and password.
-
On the Unit List page, select the Symbio 700 controller to pair with. If the controller is not listed, press the refresh arrow in the upper right-hand corner of the screen.
- When prompted, pair the app to the Symbio 700 controller. A popup message displays a 6-digit
random number. The same number is shown on the display of the Symbio 700 controller until the
pairing is complete, allowing the user to confirm the connection to the intended controller.
Bluetooth pairing - Press [Check Mark - √] on the Symbio 700 onboard keyboard/display to complete the pairing.
When the LED light is a solid blue and the display reads Bluetooth Connected, the Bluetooth pairing and
connection is complete.
Troubleshooting
| Issue | Description |
|---|---|
| Smart device requirements not met |
|
| Multiple users attempting to connect to the controller via Bluetooth |
Only one user can connect to the Symbio 700 controller via Bluetooth. If the blue light is solid, another user is connected to the controller. |
| Device outside of Bluetooth range limits | Bluetooth has physical range limitations. A user can lose connectivity if too far away from the controller and will need to re-access connectivity from the Units List page. |
| Exceeded limit of equipment pairings |
The app only allows 10 saved pairings per device.
|
| Smart device unpaired or disconnected from controller |
|
Bluetooth Operation
Bluetooth is a short-range wireless communication technology that allows electronic devices to communicate without the need for wires or cables. The Symbio 700 controller uses Bluetooth to communicate with the Symbio Service and Installation Mobile App for initial startup and servicing. For more information about the Symbio 700 Bluetooth download the pdf below.
Below is an overview of the expected Bluetooth operation on the Symbio 700.
| Action | Outcome |
|---|---|
| Pressing the Bluetooth button on the Symbio 700 controller when the blue LED is off. | Starts the Bluetooth radio for pairing for 5 minutes. The blue LED will start flashing on the controller signaling the radio is ready for connection. If a device is not paired within the 5-minute window the Bluetooth radio is turned off, and the button must be pressed again to restart the process. If a device is successfully connected within the 5-minute window the blue LED will turn solid. |
| Pressing the Bluetooth button on the Symbio 700 when the blue LED is already flashing or solid. | The Bluetooth radio is turned off. The blue LED will turn off. |
| No activity on the Mobile app for 1 hour while connected via Bluetooth. | The Symbio 700 controller will automatically turn off the Bluetooth radio after 1 hour of no activity. The blue LED will turn off. This will break the connection to the mobile app, and reconnecting will be required. |
| Walking away from the Symbio 700 controller while connected via Bluetooth. | If you have a direct line of sight to the controller the Bluetooth range is approximately 25 feet. Without a direct line of sight to the controller, the range will vary depending on the type of obstructions. If you are outside of the Bluetooth range, the connection will be lost, and reconnecting will be required. The blue LED will be flashing when the connection is lost to the mobile app. |
Click the e-library symbol for the latest version
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.