Overview
There are also alternative methods to format a USB drive to FAT32, depending on your operating system.
The FAT32 format is available on USB drives with a capacity of 32GB or less.
Formatting Steps
Step 1 - Insert the USB drive and then left-click on the Windows icon on the lower left side
Step 2 - Left-click on This PC
Step 3 - Look at the devices and drives; you should see a USB drive
Step 4 - Right-click on the USB drive; a window will pop up
Step 5 - Find Format in the window that popped up
Step 6 - Go to File System, go to the drop-down menu, and choose FAT32
Step 7 - Once FAT32 is selected, click on Start and follow the steps after
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.