- Attached is C-Series Units /error codes /OD Unit IOM /Product catalog .
- Indoor Unit IOM's can be found on E-library by typing in first four of the Model numbers.
- These are one to one units, One OD and One ID ONLY.
- Tech support has the Firmware for the OD Eeproms .
C-Series U Match , 4TUK,4MUD, 4MUC, 4MUW/ Trane Branded Samsung 1 To 1
Articles in this section
- VRF SC GATEWAY CONNECTION W/O SILVERLIGHT
- Trane Branded Samsung Water Source IOM
- Trane Branded Samsung Warranty Information
- Trane Branded Samsung cassette IOM'S /Catolog/Panel instructions
- Mode Control Unit (MCU
- VRF AUTO PORT PAIRING
- Air Handling Unit (AHU) Application Kit
- E320 Error Code for C-Series and Mini VRF units
- Outdoor Unit Operating Priority
- C-Series U Match , 4TUK,4MUD, 4MUC, 4MUW/ Trane Branded Samsung 1 To 1