Cooling:
Unit will look at zone sensor space temp input, set-point, and rate of fall. The unit will use this information in an algorithm to calculate a discharge air set-point. This is not a user controlled set-point, but can be altered by the DA Cool set-point limit being set to high or the zone sensor location receiving incorrect space temperature or incorrect information from the Discharge temp sensor. The unit is monitoring performance to help reduce unnecessary capacity run time. The unit will vary the compressor and indoor fan capacity to meet the discharge temp set-point.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.