- *LCU wiring Voyager 2 Power Exhaust Line Voltage if the unit has a VFD?
On units with a factory installed variable frequency drive (VFD), route the long, dual, high-voltage wires to the VFD Power terminal block (VTB) located inside the fuse enclosure which is mounted either underneath the VFD on horizontal units, or on the side of the VFD enclosure on downflow units . Bundle any excess wire in the corner near the access-door opening, away from the blower housing, and secure into place.
Connect the two (2) high voltage wires to the VFD Power terminal block (VTB), matching wire colors to those found on the VTB-D; red-to-red and VTB-B; black-to-black.
The Power Exhaust High Voltage wires need to be on the INPUT (L1, L2, L3) side before the fuses.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.