- Place a jumper from TEST 1 to TEST 2 on the Low Voltage Terminal Board.
- The unit will run in each mode for 30 seconds, scrolling through all modes (relevant to that specific model). It will exit test mode automatically.
- To go through test mode again simply remove (for ~2 seconds) and restore the jumper.
- If the jumper is removed at any time during the test mode, the unit will stay in the currently selected mode for 1 hour (except for the defrost mode on heat pumps). After 1 hour it will automatically exit test mode and resume normal unit operation.
- Only stages for which the unit is designed will be activated. All others will be skipped.
Table 1. Test Stages
| Test Stage/Step | Test Mode |
|---|---|
| 1 | Indoor Fan On |
| 2* | Economizer Open |
| 3 | Cool 1 |
| 4* | Cool 2 |
| 5* | Cool 3 |
| 5 | Heat 1 |
| 6* | Heat 2 |
| 7* | Heat 3 |
| 9* | Heat 4 |
| 8** | Defrost Cycle/Reheat |
| 9* | Emergency Heat |
* Optional components ** Defrost cycle in test mode runs for at least 1 minute and up to 10 minutes depending on outdoor ambient and outdoor coil temperatures. ** Reheat is only valid with dehumidification option and will be initiated directly after the last Cool stage. | |
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.