When working with LCI-R and LCI-RX XIF files, it is important to have a clear understanding of the data structure and the meaning of the different metadata fields.
- LCI-RX XIF, version 6, 80 00 2A 50 00 03 04 0E
- LCI-RX XIF, version 7, 80 00 2A 55 00 03 04 0F
- LCI-RX XIF, version 8, 80 00 2A 55 00 03 04 10
- The XFB file is a binary form of the XIF
Notes:
- The LCI-RX v8 will not work with RTRM v6
- The RTRM v6 will make the LCI-RX applicationless, and the LCI-RX will have to be replaced.
- If you are putting an LCI-RX on a ReliaTel rooftop with RTRM v6 or older, you will also have to replace the RTRM.
- This might also be true with an RTRM v7 or newer, unsure where the cutoff is.
- RTRM v23 works with the new LCI-RX.
See below link for the installation guide
E-Library: ACC-SVN175* - Trane Commercial (tranetechnologies.com)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.