The zone sensors that are compatible with the Symbio 700 are
BAYSENS108
BAYSENS077
BAYSENS135
BAYSENS135-Connections-to-a-Symbio-700
BAYSENS800 Only the advance Symbio board is capable of using this sensor.
Connecting-a-BAYSENS800-to-an-Odyssey-Symbio-700-Controller
Zone sensors that are not compatible are the BAYSENS119 and BAYSENS924.
Click the e-library symbol for the latest version
Click the e-library symbol for the latest version
Click the e-library symbol for the latest version
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.