This needs to be done with the app installed on phone Where-to-get-the-Symbio-700-Phone-App
Once the app is installed on the phone and you are connected to the device follow these steps to change the Device ID and/or Buad Rate.
Step 1: Home page of the app go to tools on the bottom right side.
1.
Step 2: Check on Protocal Configuration
2.
Step 3: To change the device ID or Buad rate Click edit upper right corner
For Buad rate skip to Step 5.
3.
Step 4: To edit software Device ID change to Yes. Once it is yes then you can change the Device ID
4A and once that is changed then you can save it the save it 4B which is on the upper right hand side
and it will be green in color.
4.
4A and 4B
Step 5: To change the Baud Rate click on Edit. Once you Click on 5A edit
Baud Rate will be green and you can change it once changed sve it 5B upper
righthand corner will have save and it will be green.
5.
Step 5A and 5B
5A and 5B
For more information you can watch a video
https://www.youtube.com/watch?v=mWIlsp0Tclg&list=PLXixdXQF2g5XR-Bz7EFMLYCGe3CGTanje
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.