Table of Contents
Daytime Warm-Up
Daytime Warm-up is a feature of VVDA units that can be enabled or disabled. Daytime Warm-up is available with any heat type installed. Daytime Warm-up is a mode used during building occupied periods to recover a critical zone that is too cold. Ventilation air is provided while in Daytime Warm-up mode.
When the Heat Cool Mode Request is Cool (the unit is providing cooling), if a valid space temperature is 3°F below the adjustable Daytime Warm-up Setpoint, daytime Warm-up operation initiates. The unit will operate in a discharge air control mode, delivering heating capacity per Discharge Air Heating Setpoint Active. The supply fan operates at max speed on Constant Volume Units. Variable air volume discharge air control units will operate the supply fan to the duct static pressure setpoint and Heat Cool Modes report Heat Cool Mode Status as Heat, if the installed heat type allows modulating air flow. Else if the heat type requires full air flow, Maximum Heat is reported. (See Heat Types and Maximum Heat section for more information).
When the space temperature is equal to or above the Daytime Warm-up Setpoint, the daytime Warm-up operation terminates, and the Symbio™ 700 will transition back to Cool mode. See Maximum Heat for details. If the requested operating mode is no longer Cool, Daytime Warm-up terminates.
Application Guide Link
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.