This is one of the design features of the 5 ton and below Axiom horizontal water source heat pumps. It is as simple as changing panels. The panel that is taken off on the new location will replace the panel where the blower originally was.
It is important that pay attention to the serviceability of the fan motor. In some cases, it may be necessary to rotate blower panel 180 degrees to have accessibility to the fan.