There are several reasons why a unit will not start, the purpose of this article is to step you through common troubleshooting steps and get your unit running.
Resolution
- Make sure your line voltage is within 10% of unit rating.
- Check to see if the unit is equipped with a water stainer, check the condition, and clean as needed.
- Verify secondary voltage at the unit control transformer(s).
- Voltage should be 25-27vac.
-
See what control is installed on your unit and continue with the appropriate steps below.
24v Deluxe - Does the unit have a remote shutdown wired such as a fire alarm?
- Does the control have error codes?
- Does the unit have a condensate overflow?
- Does the unit have a call from the thermostat/space controller/zone sensor?
- Verify 24v to ground on G, Y1, Y2 (where applicable) and O (powered for cooling).
- See unit diagram for more information.
- Diagrams are located in the unit installation / operation / maintenance manual.
Recommended conventional thermostats for WSHP with 24v Deluxe controls
- Verify the unit has a wired sensor or a value is being communicated via the BAS.
- The links below can be used for wiring various Trane zone sensors
- If sensor value is being communicated to a UC400, someone with Tracer TU will need to access the control to verify the value is reported correctly.
- If the unit has Symbio 500 / 400-B, check to see if the point is in fault. See step 6.
- Verify 24v to ground on G, Y1, Y2 (where applicable) and O (powered for cooling).
WARNING
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.