Suggestions/ Notes
- 5/8" Nylon brush is recommended.
- (1) replacement O-Ring Per condenser. RNG00070.
- Do not use petroleum base grease on O-Ring
- Torque the clamps on the condenser barrel to 45 ft lbs.
Condensing water contains minerals that collect on the condenser tube walls. Cooling towers also collect dust and foreign materials that deposit in the condenser tube. The formation of scale or sludge in the condenser is indicated by a decreased water flow, low temperature difference between inlet and outlet water, and abnormally high condensing temperatures. To maintain maximum condenser efficiency, the condenser must remain free of built-up scale and sludge. Clean the condenser either mechanically or chemically.