Symbio Firmware can be updated in the field without the need for Tracer TU. Users will need a USB A to B cable (printer cable), a laptop and the firmware.
Steps to update the Symbio Firmware using the built in Web UI
-
Download the latest Symbio Firmware from the Trane Software Downloads Site to a known place on your PC. The download site can be found here: https://www.trane.com/commercial/north-america/us/en/products-systems/building-management---automation/trane-controls-software-downloads.html
-
Connect the USB A to B cable to the Symbio and to the laptop. The image below shows were to connect the USB cable to the Symbio.
- In a browser type or paste the following http://198.80.18.1
-
Select Log In
-
Select Tools and then select Firmware from the Tools list.
Note: It is highly recommended to backup the controller before proceeding. This can be done in the Backup and Restore options under tools. -
To select the firmware file to be uploaded to the controller, press the Select Button that is boxed in red below.
-
Browse to where the firmware file was saved in step 1, select the file. The selected file will appear in the file Name dialog in the bottom left of the screen. Select Open.
-
Select Upload
-
A popup will appear, select Continue to confirm that the device will restart.
- The web UI will show Uploading followed by restarting. On the Symbio 800 the 7 segment display will show U21. This will continue for about 6 minutes followed by the controller rebooting and the seven segment display going to a dancing vertical line pattern indicating normal operation.
- Once the controller has been successfully updated, the Web UI will display Success. Select OK to continue.
The controller firmware has been successfully upgraded.