Some government facilities and high-security sites require disabling Bluetooth on the Symbio 700 board.
You can disable Bluetooth through the user interface on the Symbio 700 board by following the steps below.
Select the Home button to start the main menu
Scroll down to Utilities
Select the check mark
Scroll down until Communication is displayed
Select the check mark
Disable Bluetooth/Enter to Disable should be displayed
Select the check mark to disable the Bluetooth
Are you sure? will be displayed
Scroll down to Yes
Select the check mark
-
Bluetooth Not Allowed will now scroll across the display
Notes
The only way Bluetooth can be re-enabled is through a reset caused by:
- Changing equipment type - This will clear out the configuration and the Symbio 700 will need to be re-configured.
- Applying a backup - The backup must be before Bluetooth is disabled.
- Performing a factory reset - This will clear out the configuration and the Symbio 700 will need to be re-configured.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.