The following sensors are capable of having a remote 10K type II mounted externally from the sensor in the space for control.
- Symbio™400/UC400: X13790993 (SEN02587)
- ReliaTel™: X13790994 (BAYSENS924)
- Symbio™ 700/800: X13791009 (BAYSENS800)
Any of Trane's Zone sensors will work with this sensor will work with this sensor as they are all 10K Type II. Setpoint is not required, Sen01448 is recommended.
| Sensor Type | Features | Part number | BAYSENS | Global parts | ||||
|---|---|---|---|---|---|---|---|---|
| Setpoint | Fan Control | System | Occupancy | LEDs | ||||
| Temperature Sensors | Single | No | No | Yes | No | X1351152701 | BAYSENS974A | SEN01447 |
| No | No | X1351152801 | BAYSENS977A | SEN01448 | ||||
| Single | No | X1351152901 | BAYSENS975A | SEN01449 | ||||
| No | Yes | X1351153001 | BAYSENS973A | SEN01450 | ||||
Steps
- The sensor is wired to terminals 17 and 18 of the unit.
- The configuration of the inputs must be set as well as the type of sensor. This is done from the Configuration Menu 2/4.
To enter the menu:
Navigate to the 2/4 Configuration page
- Set the UC17 config from None to Temp
Set the Temp. sensor from Internal to Wired, DO NOT set for remote
Erase all? Resets the sensor back to factory settings. Are you sure? Confirms the erase reset. UC17 config Defines the sensor connected to electrical terminals 17 and 18.
- None - terminal not in use.
- Motion - motion sensor or external dry contact.
- Temp - 10K temperature sensor.
Temp. sensor Defines the location of the space temperature sensor used for control.
- Internal - sensor internal to the zone sensor.
- Remote - sensor wired to the HVAC equipment.
- Wired - sensor wired to zone sensor terminal 17 and 18.
Occupancy src Defines the source of the occupancy signal.
- Scheduled - zone sensor time schedule.
- Motion - motion sensor or external dry contact wired to zone sensor.
(a) The parameter is only displayed when the zone sensor is connected to a ReliaTel™ or Symbio™ 800 control system.
If multiple sensors are needed, 4 sensors must be added at one time and wired in a series parallel configuration as shown below. This is for the temperature only version of the sensor. Setpoint, Fan and On/Cancel is not supported.