If the drive is still connected to line voltage and the display is on, follow the instructions in Figure 2.
Low voltage power can be applied externally with a PC using a USB A to USB Mini B cable accessing the terminals in Figure 1. Once the display is powered, proceed to the steps listed in Figure 2 to save the parameters to the operation panel or display.
Figure 1:
Text in Figure 1, above.
- Place a flathead screwdriver, etc. in a slot and push up the cover to open.
- USB host (A connector)
- Communication status indicator (LED)
- USB device (Mini B connector)
- Personal computer (FR Configurator2)
Figure 2:
Text in Figure 2, above.
Parameter copy
- Inverter parameter settings can be copied to other inverters.
Reading the parameter settings of the inverter to the operation panel.
Operation
1. Connect the operation panel to the source inverter. 2. Parameter setting mode.
- Press MODE to choose the parameter setting mode (The parameter number read previously appears.)
3. Selecting the parameter number.
- Turn dial to
PrCPY(parameter copy), press the SET.0.— — —appears.4. Reading to operation panel.
- Turn dial to change the set value to
1Rd. Press SET to start reading of the inverter parameter settings by the operation panel. (It takes about 30 seconds to read all the settings. During reading1Rdflickers.)5. End reading
1RdandPrCPYflicker alternately after settings are read.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.