EXAMPLE:
CO2 sensor with 2 to 10 Vdc output (range 0 to 2000 ppm).
Two (2) Vdc is equal to 0 ppm, 10 Vdc is equal to 2000 ppm, and the threshold is determined to be 1000 ppm. According to the chart below, the DCV Set potentiometer is to be set at 6 Vdc.
- Adjust the DCV Set potentiometer with a small screwdriver by turning the pot to the fully CCW and then fully CW positions to determine the end stops.
- Set the pot for 6 Vdc in the mid position.
- Set Min Position Pot where you want the damper to be anytime the fan is running.
- Set the DCV Max Pot for the maximum you want the damper to be open when the CO2 in the space gets above the DCV Setpoint (1000 ppm in this example)
CO2 Sensor Output Info
2-10 Vdc Output Example.
CO₂ Level (ppm) 0 250 500 750 1000 1250 1500 1750 2000 Voltage Output (Vdc) 2 3 4 5 6 7 8 9 10 Economizer Module DCV Output vs Actuator / Damper Position (approximate)
DCV Output 2 2.8 3.6 4.4 5.2 6 6.8 7.6 8.4 9.2 10 Damper Position 0% 10% 20% 30% 40% 50% 60% 70% 80% 90% 100%
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.