Issue:
This MP501 is set up as an SCC with a two-pipe auto changeover configuration. How does the MP501 perform the changeover?
Resolution:
The MP501 is in cooling mode if nviSourceTemp is less than 75F. It is in heating mode if nviSourceTemp is greater than or equal to 75F.