Blower coil 3 phase motor with incorrect rotation. If switching the wires to the unit then the following repair must be made.
Wires P5 and P11 will have a jumper between them. Make sure that P 9 is grounded.
Remove the jumper between P5 and P11 and the motor will rotate in CCW