This article explains the sequence of operation for the heating functions available on Legacy IntelliPak units manufactured from 1993 through 2022. It covers the operating procedures and control logic associated with Morning Warmup, Daytime Warmup, supply-air tempering, and supply-air heating. The information is intended to clarify how each heating mode operates, when it is initiated, and how the unit responds to heating requirements during different stages of operation.
Morning Warm-up - IntelliPak 20-130 CV/VAV
On all VAV units equipped with heat, Morning Warm-up (MWU) allows the unit to do a one-time Constant Volume (CV) 100% airflow heating mode at the beginning of each occupied mode as needed. During this mode the economizer will be closed except as described below. MWU must be enabled, and the zone temperature must be lower than the MWU setpoint.
Setup:
MWU can be enabled/disabled through the SETUP menu on the Human Interface or through BAS/Network. On this same screen, Full Capacity or Cycling Capacity is also chosen. If MWU is enabled, the unit must have a space temperature reading sensor designated (CONTROLLING SENSOR STATUS SUBMENU) as the Morning Warmup Zone Temperature Sensor and a source specified to receive the Morning Warmup Heating Setpoint (CONTROLLING SETPOINT STATUS SUBMENU).
Operation:
Upon switching from the Unoccupied to the Occupied Mode, with MWU enabled, the unit compares the MWU Zone Temperature to the MWU Heating Setpoint. If the MWU Zone Temperature is equal to or higher than the Morning Warmup Heating Setpoint then there will be no call for heating and the unit will go into normal Occupied control.
If the MWU Zone Temperature is lower than the MWU Heating Setpoint then the unit will go into either Full Capacity or Cycling Capacity Morning Warmup (depending on SETUP). The VAV box relay output continues to be energized during MWU and is de-energized at the end of the MWU cycle.
For Full Capacity operation, a request will be sent to energize all heat stages to 100% until the MWU Temperature Heating Setpoint has been satisfied. There is no time limit. After the setpoint has been reached, the unit will go into normal Occupied control. This option provides building warm-up with the outside damper shut.
For Cycling Capacity operation the unit will energize heat stages as necessary to satisfy setpoint. Unit will operate in this mode until MWU Heating Setpoint has been satisfied or until 60 minutes have elapsed. At this point, the unit will transition into occupied mode. If the space temperature is below the Daytime Warmup (DWU) Initiate Setpoint, the unit will continue to heat in the DWU Mode (see Daytime Warm-up - IntelliPak 20-130 VAV) If the space temperature is above the DWU Initiate Setpoint, the unit will transition into discharge air cooling mode.
For units with no heat, this function may still be used to support systems with heat sources other than those provided in the rooftop unit (e.g. VAV units with reheat boxes). This is done by configuring the unit as "External Heat". The unit does not require a heat module with this configuration. The MWU cycle will terminate after 60 minutes.
Service note:
When the unit is powered up or transitioned from STOP to START such as after an External Auto-stop mode, the unit will enter a MWU mode if the zone is cooler than the MWU setpoint. If this occurs, the supply fan and heat will not come on until after the VAV BOX MAX STROKE TIME has elapsed. The factory default is 6 minutes, though this can be adjusted from 0 to 10 minutes under SETUP. After the VAV box stroke time has elapsed, the heat and fan will be allowed to start. This allows time for the VAV boxes to fully open before the supply fan starts.
Daytime Warm-up - IntelliPak 20-130 VAV
On all VAV units equipped with heat, Daytime Warm-up (DWU) may be enabled. This mode allows the unit to go to a Constant Volume 100% airflow heating mode when certain conditions are met. Here are the setpoints for this mode:
Daytime Warmup Setpoints:
Initiate: This is the zone temperature at which the unit will enter DWU mode.
Terminate: This is the zone temperature at which the unit will leave the DWU mode.
Occupied Zone Heating Temp Setpoint: This is the ACTUAL DWU Setpoint. It is the temperature to which the heat is controlled to during a DWU mode. (see note 5 below). This setpoint can come from the HI keypad setpoint menu (default), Zone Sensor Module, NSB panel, GBAS, or BAS/Network.
Setup:
DWU can be enabled / disabled through the SETUP menu on the Human Interface or through the BAS/NETWORK. If DWU is enabled, the unit must have a sensor designated (CONTROLLING SENSOR STATUS SUBMENU) as the DWU temperature sensor. Also the unit must have a setpoint source specified (CONTROLLING SETPOINT STATUS SUBMENU).
Operation:
During an occupied cooling mode, if the designated DWU sensor (zone sensor) temperature drops below the Initiate setpoint, the unit will enter DWU mode. The VAV box output (RTM K3) is energized at this time. After the VAV BOX MAX STROKE TIME has elapsed (factory set at 6 minutes), the supply fan will ramp up to maximum speed (or the inlet guide vanes will open to maximum). Next, the heat will be energized. When the zone temperature exceeds the DWU Setpoint or Occupied Zone Heating Setpoint, the heat will shut off. The heat will cycle or modulate to maintain the DWU Setpoint. When the zone temperature exceeds the Terminate setpoint, the unit will exit the DWU mode, deenergize the VAV box output and resume its occupied cooling mode.
Additional operational considerations:
1. The unit will not go into DWU mode if the Changeover contacts are closed or the Unoccupied contacts are closed.
2. Once the unit enters a DWU mode, it will not exit this mode until the Terminate setpoint has been reached. For example, the unit could go into an unoccupied mode, yet stay in DWU because the Terminate setpoint is too high.
3. The unit will exit a DWU mode if an External Auto Stop mode occurs however.
4. If the Terminate setpoint is higher than the DWU setpoint, the zone must continue to warm up by some other means (such as VAV reheat) until the Terminate setpoint is reached.
5. On units built prior to January 1, 1996, Occupied Zone Temp Setpoint was not used. The only setpoints were Initiate (heat comes on) and Terminate (heat shuts off).
6. To force the unit to 50% modulating or 1st stage only, enable Demand Limit through GBAS or BAS.
7. The initiate and terminate setpoints can only be set at the Human Interface (HI).
Service note:
Can't get the DWU Setpoint to raise above 72F? This is because the RTM has a "hidden" occupied cooling setpoint of 74F, and the heat setpoint cannot be raised above the cool setpoint. Here's how to fix it: Reconfigure the unit as a CV unit. Go into the SETPOINT menu and raise the Occupied Cooling Setpoint to a higher number such as 90F. Reconfigure the unit as a VAV unit. Now, the DWU setpoint can be raised above 72F.
Discharge Air Heating - Changeover input - IntelliPak 20-130 VAV
Changeover is used on VAV units with modulating heat, i.e. modulating gas (limited & full), hot water, and steam. This is not supply air tempering.
This mode causes the unit to heat and maintain the discharge air heating setpoint. The unit will not resume cooling until the changeover input is removed.
Changeover cannot be used to do discharge air controlled heating with staged heat, i.e. 2-stage gas or electric heat
There are two ways to initiate changeover:
1) Changeover input (field provided 5K87 connected to 1TB5-21 and 1TB5-22):
Open: Allows the unit to control to the discharge air cooling setpoint .
Closed: Allows the unit to control to the discharge air heating setpoint.
2) Through LON, use nviApplicMode HVAC_HEAT or changing the Heat Cool Mode to Heat through the BAS/Network.
Field note: During discharge air heating the VAV boxes need to be in heating mode as well. In addition to the changeover contact closure, the VAV boxes must be made to control to a local heating setpoint instead of a cooling setpoint. Otherwise, the VAV boxes will overheat the zones
Staged heat note: If the unit has 2 stage gas heat or electric heat and the changeover contacts are closed, here's what happens:
The unit is forced into a Daytime Warmup Mode (DWU) regardless of DWU setpoints. The unit will use the Occupied Zone Temp Setpoint to cycle the heat, however this CV mode will not terminate until BOTH the Terminate setpoint is reached and the changeover contacts are open. After termination has occurred, the unit will resume VAV cooling. See DWU link below for more information.
Supply Air Tempering - IntelliPak 20-130 VAV
Hot water, steam heat, or modulating gas will be modulated to prevent the Supply Air (SA) temperature from falling below the low end of the SA temperature deadband. This mode is active during the cooling mode only. All cooling stages must be off and the economizer at minimum position for this feature to operate.
For example, if the SA cooling setpoint is 55F, and the SA cooling deadband is 10F, then SA tempering will begin if the SA temperature drops below 50F with the economizer at minimum position.
During SA tempering, this lower limit becomes the tempering setpoint. The SA heating deadband becomes active to determine the proportion of heat needed. Using the example presented above, if the lower limit (also called SA tempering setpoint) is 50F, and the heating deadband is 5F, the heating output algorithm will seek to reduce the heating output at 52.5F, and will seek to increase the output at 47.5F.
Should the supply air temperature rise up to the SA cool setpoint plus 1/2 the cooling deadband, the unit will resume cooling and SA tempering mode will terminate.
Service note #1: While a tempering mode is occuring, the status screen on the Human Interface will say HEAT even though the unit is in the cooling mode.
Service note #2: Avoid SA tempering w/ modulating gas on IntelliPak with Rooftop module (1U48) version <19.00;
When the SA temperature drops to the lower limit and initiates SA tempering, the gas valve starts at 100%. Then, the signal to reduce the output is given which reduces the gas output. Since the initial output is 100%, the SA temperature can rapidly rise well above the SA cooling setpoint. Should this happen, the RTM will force the unit to start cooling. If economizing, which is usually the case, the outside air damper opens up to 100% in response to the sudden rise in SA temperature. This can cause the supply air temperature to plummet, and in turn can cause supply air tempering to initiate again. This cycle of large SA temperature fluctuation may continue, resulting in discomfort in the affected zones. For this reason, it is best to avoid using SA tempering with modulating gas. The field fix for this is to replace the RTM with a current version.
Service note #3: Rooftop module (1U48) version 19.00, released March '03, does not allow a unit to cycle out of SA tempering mode (once initiated) for the first 5 minutes.
Supply Air Tempering - IntelliPak 20-130 CV
If the supply air temperature drops 10F below the Occupied Heating Setpoint, the unit will bring on 1 stage of heat until the supply air temperature rises to 10F above the Occupied Heating Setpoint.
If the unit has a call for heating, supply air tempering will terminate before the supply air temperature rises to 10F above the Occupied Heating Setpoint.
This feature is only available with staged gas heat units.
Service Note: Supply Air Tempering can be disabled or enabled in the Setup, General Unit Functions Setup Submenu
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.