Economizer Operation with Zone Sensor, Programmable Zone Sensor, or ICS
When enabled, the economizer will modulate between minimum position and 100% to maintain the mixed air temperature to the calculated mixed air setpoint (53°F minimum). If the mixed air temperature starts to fall below the mixed air setpoint, the economizer starts closing. If the mixed air temperature falls to 50°F or below, the damper will close to the minimum position.
Economizer Operation with Conventional Thermostat
The economizer control is based strictly on a signal from the thermostat, but still maintains mixed air temperature control of 53° ±3°F when in the economizer mode. The economizer enable and disable function is still determined by the outside air sensor through the RTRM.
- Apply power to the unit.
- Place the zone sensor fan selector in the fan “ON” position and the heat/cool the selector in the “OFF” position to place the damper in the minimum ventilation position.
- Turn the Min Position potentiometer (on the rooftop economizer module [RTEM]) clockwise to open or counterclockwise to close. The damper will open to this setting each time the blower circuit is energized. When adjusting the minimum position, the damper may move to the new setting in several small steps.
- Wait at least 15 seconds for the damper to settle at the new position.
- Replace the filter access panel. The damper will close when the blower circuit is de-energized.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.