Object Naming Conventions
| Suffix | Description |
|---|---|
| Status | Points with the Status suffix are defined as read-only. The status point reports the value being used by the controller. |
| Local | Points with the Local suffix are defined as read-only. The local point reports values associated with controller sensors, both wired and wireless. The local value may or may not be actively used by the controller, depending on the presence or absence of a communicated value (BAS). When both a local and communicated value exist, the communicated value is used. |
| Active | Points with the Active suffix are defined as read-only. The active point reports the value being input to the controller. |
| Setpoint | Points with the Setpoint suffix are defined as either read-only or read/write. For BACnet®, the binary input, analog input, and multi-state input points are all read-only. These setpoints report the value currently in use by the controller. The analog value, binary value, and multi-state value points are all read/write. These points are provided for use by the building automation system (BAS). When used, these points are written internally to the arbitration logic. This defines the interaction with hardwired points, editable software configuration points, and the relinquish default value/state. Refer to the Appendix for additional information. |
| Input | Points with the Input suffix are defined as read-only. These points normally reflect the status of a sensor input, either hardwired or communicating wirelessly (AirFi®). However, the input point reflects the arbitrated result of the controller sensor input and a communicated value, if present. When both a controller sensor and communicated value exist, the controller will use and report the communicated value. |
| Arbitrator | Points with the “Arbitrator” suffix are to be used as read-only. The arbitrator prioritizes inputs from communicating points, hardwired points and stored defaults points. The priority array of the arbitration point displays each of the values provided, including the active status, indicating which of the input sources is being used. |
| BAS | Points with the BAS suffix are defined as read/write. These points are provided for use by the building automation system (BAS). When used, these points are written to arbitration logic. This defines the interaction with hardwired points, editable software configuration points and the relinquished default value/state. |
| Command | Points with the Command suffix are defined as read/write. These points are written to change the default behavior of the controller. Once written, these point values may be persisted. |
| Request | Points with the Request suffix are defined as read/write. These points are written to request a change the operating behavior of the controller. |
* For BAS, use the object value in bold blue color
Points Configuration for Space Temperature (CVZT & VVZT)
Points Configuration for Space Temperature (CVZT & VVZT)
| Object ID | Object Name | Description | Configuration Dependency | Read/ Write | Reliquish Default | Heartbeat Interval (seconds) |
|---|---|---|---|---|---|---|
MV-11100 |
Arbitration Method Request |
Setting for unit to use "Enable External/BAS Control" or "Standalone Control" data prioritization |
Always |
Write |
Enable External/BAS Control |
1 = Enable External/BAS Control 2 = Standalone Control |
BV-10104 |
Supply Fan Configuration Command |
Used to command the supply fan configuration as either cycling or continuous |
Space Controller is Configured as Single Setpoint or Dual Setpoint Zone Sensor |
Write |
Continuous |
false = Cycling true = Continuous |
BV-10109 |
Filter Timer Reset |
Command the unit to reset the accumulated filter run hours. |
Always |
Write |
Accumulating |
false = Accumulating true = Reset |
BV-10110 |
Reset Diagnostic |
Used to initiate a request to reset any controller diagnostics |
Always |
Write |
Normal |
false = Normal true = Reset |
MV-10104 |
Heat Cool Mode Request |
Used to command the unit into a heat/cool mode |
Space Controller is Configured as Single Setpoint or Dual Setpoint Zone Sensor and System Type is Configured as VVDA |
Write |
Auto |
1 = Auto 2 = Heat 3 = Morning Warm-up 4 = Cool 5 = Night Purge 6 = Pre Cool 7 = Off 8 = Test 9 = Emergency Heat 10 = Fan Only 11 = Free Cool 12 = Ice-Making 13 = Max Heat 14 = Economizer 15 = Dehumidify 16 = Calibrate |
MV-10106 |
Occupancy Request |
Normally used by the BMS to command the unit into an occupancy mode |
Space Controller is Configured as Single Setpoint or Dual Setpoint Zone Sensor and System Type is Configured as VVDA |
Write |
Auto |
1 = Occupied 2 = Unoccupied 3 = Occupied Bypass 4 = Occupied Standby 5 = Auto *Note Below 6 |
AV-10106 |
Space Temperature Arbitrator |
Indicates the space temp determined by arbitration |
Space Controller is Configured as Single or Dual Setpoint Zone Sensor |
Write |
65535°F Range 40 - 200 |
0 *Note Below 1 |
AV-10114 |
Space Temperature BAS |
Used to send the space temperature value |
Space Controller is Configured as Single or Dual Setpoint Zone Sensor |
Write |
0°F Range 40 - 200 |
900 Full BAS Control *Note Below 2 *Note below 5 |
AV-10127 |
Space Temperature Setpoint BAS |
BAS-supplied space temperature setpoint value |
Space Controller Configured as Single Setpoint Zone Sensor |
Write |
72.5°F Range 40 - 115 |
0 |
AV-10130 |
Occupied Offset |
Difference between the occupied cool and heat setpts when a single setpoint is used |
Space Controller Configured As Single Setpoint Zone Sensor |
Write |
2.5°F Range 1 - 10 |
0 |
AV-10123 |
Unoccupied Cooling Setpoint |
Used to define the cooling temp setpoint used for control in unoccupied mode |
Space Controller is Configured as Single or Dual Setpoint Zone Sensor |
Write |
85°F Range 50 - 90 |
0 |
AV-10124 |
Unoccupied Heating Setpoint |
Used to define the heating temp setpoint used for control in unoccupied mode |
Heating Installed and Space Controller is Configured as Single or Dual Setpoint Zone Sensor |
Write |
60°F Range 50 - 90 |
0 |
AV-10154 |
Space Cooling Setpoint High Limit BAS |
Space Cooling Setpoint High Limit BAS |
Space Controller is Configured as Single or Dual Setpoint Zone Sensor and System Type is Configured as VVZT or CVZT |
Write |
90°F Range 45 - 95 |
0 *Note Below 3 |
AV-10155 |
Space Cooling Setpoint Low Limit BAS |
Space Cooling Setpoint Low Limit BAS |
Space Controller is Configured as Single or Dual Setpoint Zone Sensor and System Type is Configured as VVZT or CVZT |
Write |
50°F Range 40 - 110 |
0 *Note Below 3 |
AV-10157 |
Space Heating Setpoint High Limit BAS |
Space Heating Setpoint High Limit BAS |
Space Controller is Configured as Single or Dual Setpoint Zone Sensor and System Type is Configured as VVZT or CVZT and Primary Heating is Configured |
Write |
80°F Range 40 - 105 |
0 *Note Below 3 |
AV-10158 |
Space Heating Setpoint Low Limit BAS |
Space Heating Setpoint Low Limit BAS |
Space Controller is Configured as Single or Dual Setpoint Zone Sensor and System Type is Configured as VVZT or CVZT and Primary Heating is Configured |
Write |
50°F Range 40 - 105 |
0 *Note Below 3 |
AV-11140 |
Discharge Air Cooling Setpoint (Target) |
Discharge Air Cooling Setpoint (Target) |
System Type Configured as VVZT and Space Controller is Configured as Single or Dual Setpoint Zone Sensor |
Write |
55°F Range 40 - 80 |
0 *Note Below 4 |
AI-10218 |
Space Temperature Input |
Indicates the space temp from a wired sensor. |
Space Controller is Configured as Single or Dual Setpoint Zone Sensor |
Read |
Range 40 - 200 |
N/A Using Zone Sensor |
AI-11159 |
Space Temperature Cooling Setpoint Input |
Indicates the (occupied) cooling setpoint from the connected wired space sensor |
Space Controller Configured as Dual Setpoint Zone Sensor |
Read |
Range 52 - 95 |
N/A *Note Below 5 |
AI-11160 |
Space Temperature Heating Setpoint Input |
Indicates the (occupied) heating setpoint from the connected wired space sensor |
Heating Source Installed and Space Controller Configured as Dual Setpoint Zone Sensor |
Read |
Range 49 - 92 |
N/A *Note Below 5 |
AI-11161 |
Space Temperature Setpoint Input |
Space Temperature Setpoint from a connected wired sensor. |
Space Controller Configured as Single Setpoint Zone Sensor |
Read |
Range 45 - 95 |
N/A |
Notes
For more information, reference the Application Guide
Points Configuration for Discharge Air Control (VVDA)
Points Configuration for Discharge Air Control (VVDA)
| Object ID | Object Name | Description | Configuration Dependency | Read/ Write | Reliquish Default | Heartbeat Interval (seconds) |
|---|---|---|---|---|---|---|
MV-11100 |
Arbitration Method Request |
Setting for unit to use "Enable External/BAS Control" or "Standalone Control" data prioritization |
Always |
Write |
Enable External/BAS Control |
1 = Enable External/BAS Control 2 = Standalone Control |
BV-10104 |
Supply Fan Configuration Command |
Used to command the supply fan configuration as either cycling or continuous |
Space Controller is Configured as Single Setpoint or Dual Setpoint Zone Sensor |
Write |
Continuous |
false = Cycling true = Continuous |
BV-10109 |
Filter Timer Reset |
Command the unit to reset the accumulated filter run hours. |
Always |
Write |
Accumulating |
false = Accumulating true = Reset |
BV-10110 |
Reset Diagnostic |
Used to initiate a request to reset any controller diagnostics |
Always |
Write |
Normal |
false = Normal true = Reset |
MV-10104 |
Heat Cool Mode Request |
Used to command the unit into a heat/cool mode |
Space Controller is Configured as Single Setpoint or Dual Setpoint Zone Sensor and System Type is Configured as VVDA |
Write |
Auto |
1 = Auto 2 = Heat 3 = Morning Warm-up 4 = Cool 5 = Night Purge 6 = Pre Cool 7 = Off 8 = Test 9 = Emergency Heat 10 = Fan Only 11 = Free Cool 12 = Ice-Making 13 = Max Heat 14 = Economizer 15 = Dehumidify 16 = Calibrate |
MV-10106 |
Occupancy Request |
Normally used by the BMS to command the unit into an occupancy mode |
Space Controller is Configured as Single Setpoint or Dual Setpoint Zone Sensor and System Type is Configured as VVDA |
Write |
Auto |
1 = Occupied 2 = Unoccupied 3 = Occupied Bypass 4 = Occupied Standby 5 = Auto *Note Below 1 |
AV-10121 |
Discharge Air Cooling Setpoint BAS |
Used to request the discharge air temp cooling setpoint value |
System Type is Configured as VVDA |
Write |
55°F Range 40 - 80 |
0 |
AV-10122 |
Discharge Air Heating Setpoint BAS |
Used to request the discharge air temperature heating setpoint value |
System Type is Configured as VVDA and Primary Heat is Configured or Conventional Thermostat with modulating gas heat installed. |
Write |
85°F Range 50 - 90 |
0 *Note Below 2 |
AV-10143 |
Duct Static Pressure Setpoint BAS |
Used to request the duct static pressure setpoint value |
System Type is Configured as VVDA |
Write |
1" W.C. Range 50 - 3.5 |
0 |
AV-10123 |
Unoccupied Cooling Setpoint |
Used to define the cooling temp setpoint used for control in unoccupied mode |
Space Controller is Configured as Single or Dual Setpoint Zone Sensor |
Write |
85°F Range 50 - 90 |
0 |
AV-10124 |
Unoccupied Heating Setpoint |
Used to define the heating temp setpoint used for control in unoccupied mode |
Heating Installed and Space Controller is Configured as Single or Dual Setpoint Zone Sensor |
Write |
60°F Range 50 - 90 |
0 |
Notes
For more information, reference the Application Guide
Morning & Daytime Warmup
Morning & Daytime Warmup
| Object ID | Object Name | Description | Configuration Dependency | Read/ Write | Reliquish Default | Object States |
|---|---|---|---|---|---|---|
BV-10112 |
Morning Warmup Enable Command |
Normally used by the BMS to enable morning warmup |
Space Controller is Configured as Single Setpoint or Dual Setpoint Zone Sensor or System Type is configured as VVDA and Primary Heat is Installed |
Write |
Disabled |
false = Disabled true = Enabled |
BV-10111 |
Daytime Warmup Enable Command |
Used to enable daytime warmup |
System Type is Configured as VVDA and Primary Heat is Configured. |
Write |
Disabled |
false = Disabled true = Enabled |
AV-10141 |
Morning Warmup Setpoint BAS |
Defines the space temp below which MWU is enabled |
Primary Heating Source is Configured and Space Controller is Configured as Single or Dual Setpoint Zone Sensor |
Write |
70°F Range 50 - 90 |
N/A *Note Below 1 |
AV-10149 |
Daytime Warmup Setpoint BAS |
Defines the space temp below which daytime warmup will be enabled |
System Type is Configured as VVDA and Primary Heat is Configured. |
Write |
68°F Range 50 - 90 |
N/A *Note Below 2 |
AV-10122 |
Discharge Air Heating Setpoint BAS |
Used to request the discharge air temperature heating setpoint value |
System Type is Configured as VVDA and Primary Heat is Configured or Conventional Thermostat with modulating gas heat installed. |
Write |
100°F Range 50 - 158 |
N/A *Note Below 3 |
Notes
For more information, reference the Application Guide
Economizer
Economizer
Object ID |
Object Name |
Description |
Configuration Dependency |
Read/ Write |
Reliquish Default |
Heartbeat Interval (seconds) |
|---|---|---|---|---|---|---|
AV-11132 |
Design Minimum OA Damper Position at Min Fan Capacity |
Design Minimum OA Damper Position at Min Fan Capacity |
Outside Air is Configured as 0-100% and Indoor Fan Type is Configured as Variable Speed or Multi Speed |
Write |
25% Range 0 - 100 |
0 *Note Below 1 |
AV-11131 |
Design Minimum OA Damper Position at Mid Fan Capacit |
Design Minimum OA Damper Position at Mid Fan Capacity |
Outside Air is Configured as 0-50% Motorized Damper or 0-100% and Indoor Fan Type is Configured as Variable Speed |
Write |
15% Range 0 - 100 |
0 *Note Below 1 |
AV-11130 |
Design Minimum OA Damper Position at Full Fan Capacity |
Design Minimum OA Damper Position at Full Fan Capacity |
Outside Air is Configured as 0-100% |
Write |
10% Range 0 - 100 |
0 *Note Below 1 |
AV-10144 |
Economizer Minimum Position Setpoint BAS |
Used to request the ecominizer minimum position setpoint |
Outside Air is Configured as 0-50% Motorized Damper or 0-100% |
Write |
25% Range 0 - 50 |
0 *Note Below 2 |
Notes
For more information, reference the Application Guide
Demand Controlled Ventilation
Demand Controlled Ventilation
Object ID |
Object Name |
Description |
Configuration Dependency |
Read/ Write |
Reliquish Default |
Heartbeat Interval (seconds) |
|---|---|---|---|---|---|---|
AV-10175 |
Space CO2 High Limit |
Used to define the CO2 high limit, for ventilation purposes |
Demand Controlled Ventilation is Configured as Installed |
Write |
1100 PPM Range 1000 - 2000 |
0 *Note Below 1 |
AV-10176 |
Space CO2 Low Limit |
Normally provided by the BMS to define the CO2 low limit |
Demand Controlled Ventilation is Configured as Installed |
Write |
400 PPM Range 300 - 1900 |
0 *Note Below 1 |
For more information, reference the Application Guide
0 to 50 percent Motorized Damper
0 to 50 percent Motorized Damper
Object ID |
Object Name |
Description |
Configuration Dependency |
Read/ Write |
Reliquish Default |
Heartbeat Interval (seconds) |
|---|---|---|---|---|---|---|
AV-11286 |
Motorized Damper Position Setpoint |
Motorized Damper Position Setpoint |
Outside Air is Configured as 0-50% Motorized Damper |
Write |
10% Range 0 - 50 |
0 |
AV-10144 |
Economizer Minimum Position Setpoint BAS |
Used to request the ecominizer minimum position setpoint |
Outside Air is Configured as 0-50% Motorized Damper or 0-100% |
Write |
25% Range 0 - 50 |
0 *Note Below 1 |
AI-11148 |
Remote Minimum Position |
Hardwired remote minimum position for OA damper control. |
Remote Minimum Position is Configured as Installed |
Read |
N/A |
N/A *Note Below 2 |
Notes
For more information, reference the Application Guide
Relief Damper Control - Power Exhaust
Relief Damper Control - Power Exhaust
Object ID |
Object Name |
Description |
Configuration Dependency |
Read/ Write |
Reliquish Default |
Heartbeat Interval (seconds) |
|---|---|---|---|---|---|---|
AV-10168 |
Relief Enable Position Setpoint |
The OA damper position above which the Relief sequence is enabled |
Space Pressure Control is Configured |
Write |
25% Range 0 - 100 |
0 *Note Below1 |
Dehumidification - Hot Gas Reheat
Dehumidification - Hot Gas Reheat
Object ID |
Object Name |
Description |
Configuration Dependency |
Read/ Write |
Reliquish Default |
Object States |
|---|---|---|---|---|---|---|
BV-10106 |
Dehumidification Enable Command |
Normally used by the BMS to disable unit dehumidification |
Hot Gas Reheat is Configured as Installed |
Write |
Auto |
false = Disabled true = Auto |
Notes
Dehumidification control is a mode of Cooling when hot gas reheat is configured. Symbio™ 700 supports three configurable dehumidification control options: Dew Point (default), Relative Humidity, or Humidistat control for occupied and unoccupied operation.
The following Symbio 700 points are provided for dehumidification control.
- Unoccupied Dehumidification Enable BAS (BV-11261), the default setting is Enabled for unoccupied dehumidification to operate based on the configured dehumidification control option. This setting is editable and when set to Disabled will disable dehumidification during unoccupied mode.
- Dehumidification Status (BV-11255), binary status value that reports dehumidification control is Active or Inactive.
- Dehumidification Control Status (AV-11281) reports the hot gas reheat valve status.
Dehumidification Disable Space Temperature Setpoint (AV-11398), is for CVZT/VVZTcooling only units without heat installed or VVDA units with a space temperature. If space temperature falls below this setpoint (default setting is 68°F), dehumidification disables.
Dew Point
Symbio 700 references Space Temperature Active and Space Humidity Active to calculate Space Dew Point. Likewise, Outdoor Air Temperature Active and Outdoor Air Humidity Active are referenced to calculate Outdoor Air Dew Point.
| Instance | Name |
|---|---|
| AV-11178 | Space Temperature Active |
| AI-10116 | Space Humidity Active |
| AI-10226 | Space Dew Point |
| AV-11338 | Space Dew Point Setpoint Active |
| AV-10228 | Space Dew Point Unoccupied Setpoint Active |
| AV-11113 | Space Dehumidification Setpoint Offset BAS - Active |
| AI-10118 | Outdoor Air Temperature Active |
| AI-10120 | Outdoor Air Humidity Active |
| AI-10117 | Outdoor Air Dew Point |
| AV-11341 | Outdoor Air Dew Point Setpoint BAS – Active |
| AV-11321 | Dew Point Setpoint Offset |
| AV-11342 | Unoccupied Dehumidification Timer |
Relative Humidity
Occupied dehumidification control initiates when the Space Humidity Active is greater than the Space Dehumidification Setpoint BAS - Active. Occupied dehumidification terminates when Space Humidity Active is less than Space Dehumidification Setpoint BAS - Active minus Space Dehumidification Setpoint Offset BAS - Active.
| Instance | Name |
|---|---|
| AV-11178 | Space Temperature Active |
| AI-10116 | Space Humidity Active |
| AV-11136 | Space Dehumidification Setpoint BAS - Active |
| AV-10214 | Space Dehumidification Unoccupied Setpoint Active |
| AV-11113 | Space Dehumidification Setpoint Offset BAS - Active |
Humidistat
Dehumidification operation initiates when Customer Options Module, Humidistat binary input is active. When Humidistat is used for Dehumidification control, compressors stage to 100% cooling capacity. Dehumidification operation terminates when Customer Options Module, Humidistat binary input is inactive. Reheat Humidistat Input (BI-11143) reports the status of the hardware input. If a Space Relative Humidity sensor is installed, the Humidistat input will be ignored.
For more information, reference the Application Guide
Heat Pump Heating Lockout
Heat Pump Heating Lockout
Object ID |
Object Name |
Description |
Configuration Dependency |
Read/ Write |
Reliquish Default |
Heartbeat Interval (seconds) |
|---|---|---|---|---|---|---|
AV-11274 |
Heat Pump Heating Lockout Setpoint |
Setpoint at which to disable heat pump heating based on outdoor air temperature. |
Heat Pump Systems |
Write |
0°F Range (e) - 45 |
0 *Note Below1 |
For more information, reference the Application Guide
VVAD/MZVAV Supply Air Temperature Reset
VVAD/MZVAV Supply Air Temperature Reset
Discharge Air Cooling and Heating Reset (Follow the instructions on the link provided below)
Occupancy Status Definitions
Occupancy Status Definitions
| Occupied | The controller operates in an occupied mode providing temperature and ventilation control to the occupied heating and cooling setpoints. |
| Unoccupied | The control is typically shut down and does not provide temperature control to the normal occupied setpoints. No ventilation is provided. Temperature control is determined by energy conservation and building protection thresholds. |
| Occupied Bypass | The control is temporarily in an Occupied state for a specified period and will automatically return to unoccupied operation when the bypass timer expires. The Occupied Bypass Timer is user-adjustable; setting the timer to 0 minutes effectively disables Timed Override function at the equipment controller. |
| Occupied Standby | Space temperature control units in an Occupied Standby state control to occupied heating and cooling standby temperature setpoints. Standby does not apply to controllers configured for discharge air control (such as VVDA), which will translate Standby into an Occupied status. |
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.