Issue:
Tracker is showing zone temperature for a Voyager that has the zone temperature sensor removed. Where is it coming from?
Resolution:
Â
When the temperature sensor is removed from the RTRM (J6-1,2), a failure should immediately be seen at the Tracker/CCP. A value cannot be communicated or bound for this propety.
Verify you're looking at the correct Voyager. Try rebooting the unit.
Â
Notes:
Â
Changes:
Â
Other Question/Problem/Cause Statements:
- Tracker is showing zone temperature for a Voyager that has the zone temperature sensor removed. Where is it coming from?
Facts:
- VARITRAC III CENTRAL CONTROL PANEL (CCP)
- Tracker BMTK
- VariTrac III Central Control Panel (CCP)
Original wave: wave944
Document Identifier: DOC-79127
Document Identifier: 79127