Issue:
What type of wire is recommended for Tracker BMTK or VariTrac III CCP communication links?
Resolution:
Â
For the Comm4 link on the VariTrac III, you may use
    -  Level 4 shielded wire
          length limit is reduced to 3500 feet
    - "Purple" 18 gauge, twisted pair, 23 picofarads/foot, shielded wire
         length limit is 5000 feet
You may not use Level 4 unshielded wire on the Comm4 link.
For the LonTalk link, you may use:
    -  Level 4 unshielded
          preferred
           daisy chain
         105 ohm terminator at each end of wire
    -  Level 4 shielded
         acceptable, convenient if using same wire for Comm4 link on the VariTrac III
         daisy chain
         105 ohm terminator at each end of wire
    -  "Purple" 18 gauge, twisted pair, 23 picofarads/foot, shielded wire
         acceptable, but discouraged
         daisy chain
         82 ohm terminator at each end of wire
Do not mix wire types on a communications link.
Â
Notes:
Changes:
Other Question/Problem/Cause Statements:
- What type of wire is recommended for Tracker BMTK or VariTrac III CCP communication links?
- What is the wire spec for Tracker document.
- What type of wire to use for Tracker communication link?
- What wire should be used for the CCPIII
Facts:
- Tracker BMTK
- VariTrac III Central Control Panel (CCP)
Original wave: wave3541
Document Identifier: DOC-80875
Document Identifier: 80875