Issue:
Set-up for Trends in the EMTK Tracker
Resolution:
Â
This topic is covered starting on page 104 of EMTK-OG-8, Tracker Operator's Guide.
1. Connect with hyperterminal and navigate from the main menu to Trend Logs (4S)  and select Trend Log Setup (2S).
2. The Trend Log Setup Menu will be displayed. The individual trends are shown along with the setup menu.Â
The fields are:Â
Trend Name, enter a name preceeded by a single quote (').
Trend Time Interval, values can be 1,5,15,30,60.
Start Time, the format is HR:MN AM (or PM).
Stop Time, the format is HR:MN AM (or PM).
Device Type, get value from Table 15 on page 105.
Device Number, the number of the device, ie. voyager #3.
UCM Number, if the Device type is a CCP this is the number of the UCM under that CCP.
Device Index, get the value from Tables 16Â - 20 on page 106.
3. Trends can be viewed with the Trend Log Status Menu (4S) under the Main menu.
Â
Notes:
Â
Changes:
Â
Other Question/Problem/Cause Statements:
- Trend setup
- Tracker trends
Facts:
- Tracker EMTK
Original wave: wave7066
Document Identifier: DOC-78041
Document Identifier: 78041