Issue:
How to reset a Tracker and VariTrac CCP to factory defaults
Resolution:
From the Operator Display, Advanced button/Service and Testing/Return to Factory Defaults.
For the CCP III and the Tracker BMTK, you can also hold down the two buttons on the board for 30 seconds. This will put it into a boot mode requesting image. You will then need to connect to your PC software and it will immediately start downloading code after the connection is made.
Notes:
Â
Changes:
Â
Other Question/Problem/Cause Statements:
- How to reset a Tracker and VariTrac CCP to factory defaults
- The new Tracker 24 can't see all the Voyagers. What can I do?
- Can I reset to factory defaults from the Operator Display?
- Can I restore to factory defaults from the main board?
Facts:
- Tracker BMTK
- VariTrac III Central Control Panel (CCP)
Original wave: wave1078
Document Identifier: DOC-78233
Document Identifier: 78233