Problem
Water soured heat pump applications with variable speed compressor may overcool or overheat the space. This is often associated with applications having low heating or cooling demand.
Resolution
Extended time at compressor low speed (Oil Recovery Mode) is a control feature that monitors compressor run time and output. When the compressor operates for 90 continuous minutes at the minimum speed, the compressor speed shall ramp to 50% for 3 minutes and then will be released back to normal operation. This is to ensure that oil is getting back to the compressor.
WARNING
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.