Problem: The field needs a startup checklist and manual for the factory-provided TR150
Solution: The factory VFDs are commissioned at the factory, so they are fully operated and checked according to the selection.
Note:
Parameter # 5-10 is set to Start
Parameter # 5-11 is set to No Operation
Technical Support Process - TR Series VFDs (Danfoss)
First Tier Troubleshooting with Trane Technical Support: 1-877-788-7263, have equipment serial number available. Once determined to be a drive issue, see below.
Troubleshooting with Danfoss TR Support: 1-877-872-6363, have the VFD serial number available. Danfoss will ask for your Trane Support Ticket #, which is issued when Tier I support communication is initiated.
Click the e-library symbol for the latest version
Startup Parameters on Page 122
Click the e-library symbol for the latest version
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.