Error code P6/P7: Discharge temperature protection for system A/B
Possible Cause
- EEV/filter drier/indoor coil blocked
- Under charged
- Indoor unit motor stopped abnormally
- Poor heat exchange on the outdoor coil
- Discharge temperature sensor (T5) fault
Troubleshooting
- If the ambient temperature is beyond 125°F - no need to have service
- If the T5 sensor fails - replace the sensor
- If the unit is under charge - adjust the refrigerant
- If there is poor heat exchange on the high-pressure side - correct it
- If there is a blockage - correct it
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.