The purpose of this article is to show how to connect a Smoke Detector or other shutdown device. E-stop should not be used as an option for this model unit.
To install the smoke detector or safety device Cut JP1 on the Main Board and wire Normally Closed Contacts on CN7 and CN31. If a second smoke detector is used the CN28 and CN30 should be used and the JP2 will need to be cut.
Remove the jumper and install the device with a NC dry contact here. The CN7 has 12 vdc going out through the NC contacts and returns on the CN28 terminal.
DO NOT apply outside voltage to these terminals. Applying voltage will cause board failure.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.