Display reads EA error code. This error code is related to the outside air temperature side. (T4)
Possible Cause
- T4 sensor is short or open
- T4 sensor is out of calibration
- T4 sensor is plugged into the wrong location on the board. Sensor plugs in on CN23 on the Main Board.
Troubleshooting
- OHM the T4 sensor and see if it is shorted to ground. If shorted replace sensor.
- OHM the T4 sensor and see if it is open, if open replace sensor.
- If the sensor is verified and the wiring tests out good, remove the sensor and check the OHM chart against ambient temperature with it removed. You can also drop the sensor in ice to verify is against the chart at 32 ℉. If sensor does not match chart, replace sensor.
- If all the above are correct, then replace the Main Board.
Chart
| °F | °C | kΩ | °F | °C | kΩ | °F | °C | kΩ | °F | °C | kΩ | °F | °C | kΩ |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| 0 | -17.8 | 92.005 | 41 | 5.0 | 25.925 | 82 | 27.8 | 8.849 | 123 | 50.6 | 3.514 | 164 | 73.3 | 1.575 |
| 1 | -17.2 | 89.067 | 42 | 5.6 | 25.201 | 83 | 28.3 | 8.637 | 124 | 51.1 | 3.441 | 165 | 73.9 | 1.547 |
| 2 | -16.7 | 86.042 | 43 | 6.1 | 24.500 | 84 | 28.9 | 8.432 | 125 | 51.7 | 3.370 | 166 | 74.4 | 1.519 |
| 3 | -16.1 | 83.225 | 44 | 6.7 | 23.822 | 85 | 29.4 | 8.232 | 126 | 52.2 | 3.301 | 167 | 75.0 | 1.492 |
| 4 | -15.6 | 80.512 | 45 | 7.2 | 23.165 | 86 | 30.0 | 8.037 | 127 | 52.8 | 3.233 | 168 | 75.6 | 1.465 |
| 5 | -15.0 | 77.898 | 46 | 7.8 | 22.528 | 87 | 30.6 | 7.848 | 128 | 53.3 | 3.167 | 169 | 76.1 | 1.439 |
| 6 | -14.4 | 75.390 | 47 | 8.3 | 21.912 | 88 | 31.1 | 7.664 | 129 | 53.9 | 3.103 | 170 | 76.7 | 1.413 |
| 7 | -13.9 | 72.954 | 48 | 8.9 | 21.314 | 89 | 31.7 | 7.484 | 130 | 54.4 | 3.040 | 171 | 77.2 | 1.388 |
| 8 | -13.3 | 70.615 | 49 | 9.4 | 20.736 | 90 | 32.2 | 7.310 | 131 | 55.0 | 2.978 | 172 | 77.8 | 1.364 |
| 9 | -12.8 | 68.361 | 50 | 10.0 | 20.175 | 91 | 32.8 | 7.140 | 132 | 55.6 | 2.918 | 173 | 78.3 | 1.340 |
| 10 | -12.2 | 66.180 | 51 | 10.6 | 19.631 | 92 | 33.3 | 6.975 | 133 | 56.1 | 2.860 | 174 | 78.9 | 1.316 |
| 11 | -11.7 | 64.094 | 52 | 11.1 | 19.104 | 93 | 33.9 | 6.814 | 134 | 56.7 | 2.803 | 175 | 79.4 | 1.293 |
| 12 | -11.1 | 62.073 | 53 | 11.7 | 18.593 | 94 | 34.4 | 6.658 | 135 | 57.2 | 2.747 | 176 | 80.0 | 1.270 |
| 13 | -10.6 | 60.125 | 54 | 12.2 | 18.098 | 95 | 35.0 | 6.506 | 136 | 57.8 | 2.692 | 177 | 80.6 | 1.248 |
| 14 | -10.0 | 58.246 | 55 | 12.8 | 17.618 | 96 | 35.6 | 6.357 | 137 | 58.3 | 2.639 | 178 | 81.1 | 1.227 |
| 15 | -9.4 | 56.433 | 56 | 13.3 | 17.152 | 97 | 36.1 | 6.213 | 138 | 58.9 | 2.587 | 179 | 81.7 | 1.205 |
| 16 | -8.9 | 54.683 | 57 | 13.9 | 16.700 | 98 | 36.7 | 6.072 | 139 | 59.4 | 2.536 | 180 | 82.2 | 1.185 |
| 17 | -8.3 | 52.995 | 58 | 14.4 | 16.262 | 99 | 37.2 | 5.935 | 140 | 60.0 | 2.486 | 181 | 82.8 | 1.164 |
| 18 | -7.8 | 51.366 | 59 | 15.0 | 15.837 | 100 | 37.8 | 5.802 | 141 | 60.6 | 2.438 | 182 | 83.3 | 1.144 |
| 19 | -7.2 | 49.793 | 60 | 15.6 | 15.425 | 101 | 38.3 | 5.672 | 142 | 61.1 | 2.390 | 183 | 83.9 | 1.125 |
| 20 | -6.7 | 48.275 | 61 | 16.1 | 15.025 | 102 | 38.9 | 5.545 | 143 | 61.7 | 2.344 | 184 | 84.4 | 1.105 |
| 21 | -6.1 | 46.809 | 62 | 16.7 | 14.637 | 103 | 39.4 | 5.422 | 144 | 62.2 | 2.298 | 185 | 85.0 | 1.087 |
| 22 | -5.6 | 45.393 | 63 | 17.2 | 14.260 | 104 | 40.0 | 5.301 | 145 | 62.8 | 2.254 | 186 | 85.6 | 1.068 |
| 23 | -5.0 | 44.026 | 64 | 17.8 | 13.894 | 105 | 40.6 | 5.184 | 146 | 63.3 | 2.211 | 187 | 86.1 | 1.050 |
| 24 | -4.4 | 42.705 | 65 | 18.3 | 13.539 | 106 | 41.1 | 5.070 | 147 | 63.9 | 2.168 | 188 | 86.7 | 1.033 |
| 25 | -3.9 | 41.430 | 66 | 18.9 | 13.195 | 107 | 41.7 | 4.959 | 148 | 64.4 | 2.127 | 189 | 87.2 | 1.015 |
| 26 | -3.3 | 40.197 | 67 | 19.4 | 12.860 | 108 | 42.2 | 4.851 | 149 | 65.0 | 2.086 | 190 | 87.8 | 0.998 |
| 27 | -2.8 | 39.006 | 68 | 20.0 | 12.535 | 109 | 42.8 | 4.745 | 150 | 65.6 | 2.047 | 191 | 88.3 | 0.982 |
| 28 | -2.2 | 37.955 | 69 | 20.6 | 12.220 | 110 | 43.3 | 4.642 | 151 | 66.1 | 2.008 | 192 | 88.9 | 0.965 |
| 29 | -1.7 | 36.742 | 70 | 21.1 | 11.914 | 111 | 43.9 | 4.542 | 152 | 66.7 | 1.970 | 193 | 89.4 | 0.949 |
| 30 | -1.1 | 35.666 | 71 | 21.7 | 11.616 | 112 | 44.4 | 4.444 | 153 | 67.2 | 1.933 | 194 | 90.0 | 0.934 |
| 31 | -0.6 | 34.626 | 72 | 22.2 | 11.327 | 113 | 45.0 | 4.348 | 154 | 67.8 | 1.897 | 195 | 90.6 | 0.918 |
| 32 | 0.0 | 33.621 | 73 | 22.8 | 11.046 | 114 | 45.6 | 4.255 | 155 | 68.3 | 1.862 | 196 | 91.1 | 0.903 |
| 33 | 0.6 | 32.648 | 74 | 23.3 | 10.773 | 115 | 46.1 | 4.164 | 156 | 68.9 | 1.827 | 197 | 91.7 | 0.888 |
| 34 | 1.1 | 31.708 | 75 | 23.9 | 10.508 | 116 | 46.7 | 4.076 | 157 | 69.4 | 1.793 | 198 | 92.2 | 0.874 |
| 35 | 1.7 | 30.798 | 76 | 24.4 | 10.250 | 117 | 47.2 | 3.989 | 158 | 70.0 | 1.760 | 199 | 92.8 | 0.860 |
| 36 | 2.2 | 29.917 | 77 | 25.0 | 10.000 | 118 | 47.8 | 3.905 | 159 | 70.6 | 1.727 | 200 | 93.3 | 0.846 |
| 37 | 2.8 | 29.066 | 78 | 25.6 | 9.757 | 119 | 48.3 | 3.823 | 160 | 71.1 | 1.696 | |||
| 38 | 3.3 | 28.242 | 79 | 26.1 | 9.520 | 120 | 48.9 | 3.743 | 161 | 71.7 | 1.665 | |||
| 39 | 3.9 | 27.444 | 80 | 26.7 | 9.290 | 121 | 49.4 | 3.665 | 162 | 72.2 | 1.634 | |||
| 40 | 4.4 | 26.672 | 81 | 27.2 | 9.066 | 122 | 50.0 | 3.588 | 163 | 72.8 | 1.604 |
Sensor Location
Compressor Cabinet Sensor Location & Plug numbers
Main Board Plug location
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.