Error Code Pc/Pd: Evaporator freezing protection for system A/B
Possible Cause
- EEV blocked
- Poor heat exchange on the evaporating side
- Overcharged
- Low temperature on evaporating side
- Evaporator coil temperature sensor fault
Troubleshooting
- Is the ambient temperature is below 40°F and the temperature on the evaporator is below 60°F = The board is protecting the unit
- Verify if T2 sensor failed - replace T2 sensor
- Verify if refrigerant charge (overcharge) - adjust charge
- Poor heat exchange on the evaporator coil - correct it
- Is there blockage - correct it
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.