Service Bulletin UV-SVC016A-EN: HUVC
Damper Linkage
New Retrofit Campaign
General Service Bulletin UV-SVB016A-EN
Confidential Service Bulletin UV-SVC016A-EN
Subject
Horizontal Unit Ventilators Unit configuration. DIG 20 = A, G, H, J only
may not be sealing, leaving a gap of 0.25"-0.5" allowing fresh air to freely
enter the unit which could result in Low Temperature Detectors being
tripped. Unit may have slack in the UV Damper Linkage preventing the fresh air damper seal to contact
with the discharge frame.
The action described in this bulletin is NOT being taken to address a safety concern.
This is a FIX ON FAIL Retrofit
Affected Units
Horizontal Unit Ventilators Models HUVC* with 20th digit = A, G, H, or J, product code 0042, serial number
range of H19A****** through H21D*****, shipped between May 2019 and April 2021.
HUVC Damper linkage issue
Articles in this section
- A2L Sensor mounting location- VUVE
- HUVC schematics - Latest Version
- VUVE Schematics - Latest Version
- VUVE Freeze and frost stat
- Unit Vent Damper Redesign 2025
- HUVC Damper linkage Position
- HUVC Damper linkage issue
- HUVC- Not reaching high RPM
- VUVE Coil Flipping
- Expansion Valve removal process on a Trane Unit Vent