Trane Foundation low-leak economizers come with the Honeywell Jade controller with Sylk-enabled communication. The actuator must be addressed to Direct operation with Address 11 for proper operation.
Address:
To set the direction and address for the MS3110J1008 actuator, do the following and see the image below:
- Set the Range/Direction Control Selector to "C"
Set the Sylk Address Selection to "G"
click to enlarge click to enlarge
To set the address on the MS3105J3030, change the address dial to position 1, as shown in the image below.
Verify correct wiring on the actuator is also recommended prior to testing operation.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.