Click the image below for the Symbio Precedent unit ONLY to find your configuration breakdown by unit model number.
Summary:
The Symbio Service & Installation app lets users view and edit equipment settings. Follow the instructions below to view or edit the configurations of the Symbio 700 Unit Controller.
Phone App:
From the Home Page, go to the Setting Icon
Click the View Configuration tab
This page does not auto-refresh; to manually refresh, swipe down or press refresh
To edit the configuration, press the Edit button on the next window; you'll see (Stopping the Equipment) press the Proceed button and start the equipment configuration.
Model Number Break Down Example:
- Please review the (IOM) Installation, Operation, and Maintenance Manual. Let's say the unit's model number is YSJ180A3S0L02F0C0C100A0C20000000000000D0. Please take a look at the Model Number Description in the IOM.
Type part of the model in the e-library search bar.
Click the e-library symbol below to find the latest version of the IOM
These are the configurations for the model number above:
Precedent:
View Configuration Sub-Menu
Note: Configuration options may be restricted based on dependent selections.
Equipment Type - Precedent
- System Type - CVZT, VVZT, VVDA
- Space Controller - Conventional T-Stat, Single Setpoint Zone Sensor, Dual Setpoint Zone Sensor
- Indoor Fan Type - Variable Speed/Multi-Speed
- Refrigeration System – Cooling Only, Heat Pump
- Refrigerant – R410a
- Tonnage - 6, 7.5, 8.5, 10, 12.5, 15, 17.5, 20, 25
- Refrigerant Circuit - Single Manifold
- Voltage - 208/230/60, 380/60, 460/60, 575/60
- Efficiency - Standard, High
- Hot Gas Reheat - Not Installed, Modulating
- Dehumidification Control - Relative Humidity, Dew Point, Humidistat
- Primary Heating Source - Not Installed, Electric, Gas
- Primary Heating Type - Stage
- Primary Heating Stages - 2
- Outside Air - Not Installed, 0 to 100% Economizer, 0 to 50% Motorized Damper
- Economizer Type - Dry Bulb, Reference Enthalpy, Differential Dry Bulb, Comparative Enthalpy
- Demand Controlled Ventilation - Disable, Enable
- Remote Minimum Position - Not Installed, Installed
- Space Pressure Control - Not Installed, Relief Fan Only
- Clogged Filter - Not Installed, Installed
- FroStat - Installed
- Supply Air Smoke Detector - Not Installed, Installed
- Return Air Smoke Detector - Not Installed, Installed
- Condensate Overflow Switch - Not Installed, Installed
- Humidistat - Not Installed, Installed
- Humidity Sensor - Not Installed, Installed
- CO2 - Not Installed, Installed
- Discharge Temperature Sensor - Not Installed, Installed (Requirement for economizers. Units that will have it are VVZT and VVDA.)
- External Auto/Stop - Not Installed, Installed
- Ventilation Override - Not Installed, Installed
- Alarm Indicator - Not Installed, Installed
- Demand Management - None, Demand Shed, Demand Limit
- Supply Air Tempering - Disable, Enable
- Indoor Fan VFD - Ebm Papst, Mitsubishi
Odyssey:
View Configuration Sub-Menu
Note: Configuration options may be restricted based on dependent selections.
Equipment Type - Odyssey
- System Type - CVZT, VVZT
- Refrigeration System – Cooling Only, Heat Pump
- Refrigerant – R22, R410A
- Voltage - 208/230/60, 460/60, 575/60
- Efficiency - Standard, Standard B
- Tonnage - 5, 6, 6.25, 7.5, 8.33, 10, 12.5, 15, 20, 25
- Refrigerant Circuit - Single, Dual, Single Manifold
- Indoor Fan Type - Single Speed, Multi-Speed, Variable Speed (Variable Speed is the only option on VVZT)
- Space Controller - Conventional T-Stat, Single Setpoint Zone Sensor, Dual Setpoint Zone Sensor
- Evaporator Defrost Control – Enabled, Disable
- Primary Heating Source – Not Installed, Electric, Heat Pump Note For water coil configure it for electric
- Primary Heating Type - Staged
- Primary Heating Stages – 1,2
- Secondary Heating Source – Not Installed, Electric
- Secondary Heating Type - Staged
- Secondary Heating Stages – 1,2
- Outside Air - Not Installed, 0 to 100% Economizer, 0 to 50% Motorized Damper
- Space Pressure Control - Not Installed, Relief Fan Only
- Demand Controlled Ventilation - Disable, Enable
- Ventilation Override - Not Installed, Installed
- External Auto/Stop - Not Installed
- FroStat - Not Installed, Installed
- Demand Management - None, Demand Shed, Demand Limit
- Humidity Sensor - Not Installed, Installed
- CO2 - Not Installed, Installed
- Supply Air Tempering - Disable, Enable
- Discharge Temperature Sensor - Not Installed, Installed
Note: The apply button will be enabled once all options selections have been selected.
Once completed, press the Apply or √ button on the top right corner
Note:
- A complete configuration will be required during a Symbio 700 Unit Controller replacement. All the configuration items must be selected.
- Equipment can be configured through the Tracer TU, mobile service tool, or
onboard
Click the link below to Edit using Tracer TU
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.