For a hard copy please contact your local Trane Parts Center.
Trane Commercial Touch Screen Programmable Zone Sensor for Tracer UC400, ReliaTel and Symbio 800 Controls
The Trane® programmable zone sensor is a low cost control solution that meets California Title 24 requirements for stand-alone space control applications.
The programmable zone sensor is designed for use with commercial single zone ReliaTel™ controlled, Voyager™, Precedent™, and Odyssey™ systems. Its compact size, combined with a color liquid crystal display (LCD), is both aesthetically pleasing and easy to use.
Version 1
- Designed to be used with a BCI-R in a stand alone application.
- This sensor is intended to be installed on a dedicated BACnet MSTP link between one unit controller and one sensor only.
Version 2
- This sensor can be installed on a BACnet MSTP link, unique device IDs and MAC addresses are required at the sensor and unit controller.
All Versions
- This sensor is not intended to be integrated into a Trane BAS system or 3rd party BAS. There is no published points list for the sensor and no integration support with the sensor.
To determine which sensor version you have see: Touch Screen Programmable Zone Sensor - Part Numbers AND Compatibility.
This programmable sensor will work with every ReliaTel rooftop as long as it does not have an RTAM board.
The RTAM board allows the ReliaTel to do multi zone VAV control, duct static pressure control, and discharge air temp control.
- From the TD5 home screen, select Settings.
- On the Settings screen, select Setup.
- Make sure the Display Read Only Mode is Read.
- Make sure the BCI-R is version 7.00.013 and RTRM is v19 or higher.
Please check the portal or e-library to verify the attached literature is the latest version.
Part Numbers:
- UC400: X13790993001 (SEN02587)
- ReliaTel™: X13790994001 (BAYSENS924)
- Symbio™ 800: X13791009001 (BAYSENS800)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.