Can I use a regular thermostat with an E-Flex?
No, a regular 24VAC output thermostat will not work properly with an E-Flex (Variable compressor) unit. The system may seem to control but it could be sporadic and unreliable. This will also lead to a loss of compressor and indoor fan variability which can lead to a loss of temperature and humidity control. This includes Precedent and Voyager units.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.