Technically yes, but operationally no.
- A regular 24VAC output thermostat will technically work with a Single Zone VAV (SZVAV) unit, but it will not provide variable supply air. Instead, it will actually perform as a 2-speed airflow unit. This includes Precedent, Odyssey, and Voyager units.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.