Issue(s)
- BCI-R SZVAV with wireless communications will not bring on cooling
- BCI-R SZVAV receiving a communicated space temp BAS will not bring on cooling.
- E-Flex will not bring on cooling
Problem
- BCI-R SZVAV has no problem heating or economizing but has problems with mechanical cooling.
- Problem has been seen on V20 (sticker version on the board says 19.2) v21 and v23 of the RTRM
- Not sure if the if lesser versions of the RTRM are affected or not. Still under investigation.
Workaround
- Install a sensor in the return air of the RTU and wire it into terminals 1 and 2 on the RTRM.
- Could also add a jumper between J6-1 to J6-2 on the RTRM module. Jumper tells the RTRM the space temp will be communicated.
Solution
- The RTRM is not up gradable in the field, this is a hardware change.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.