Cancel Temporary Override
- To cancel temporary override press the "up arrow" or "down arrow" twice or until hours appear.
- Press the "center square" to select time and then press the "down arrow" until time is set to 0:00, then press and hold the "center square".
Change Fan Mode
- Press the "center square" once if backlight is on or twice if backlight is off.
Press the "down arrow" once, then either "side arrow" to toggle fan mode, then press the "center square".
Filter Timer Reset
- To reset the Filter Timer, press both "up arrow" and "down arrow" simultaneously for 2 seconds.
Display Setpoint
- To display the setpoint, press both "up arrow" and "down arrow" simultaneously for 2 seconds.
The 119 will display the setpoint of what mode it is in (heat or cool) ~ the setpoint it is currently
controlling to if in Auto Changeover ~ - The 119 is in "display setpoint" when there is an arrow pointing to the temperature.
Scheduling
- You can only do 10 minute intervals.
- If you modify a previously set schedule the "morning, day, evening, night" icon will not go backwards.\
- For example if you have a schedule where "evening" starts at 15:00 and the current time is 15:15
(the "evening" icon is displayed) and you modify the schedule so "day" starts at 15:30,
the 119 will not go backwards and display the "day" icon when the time reaches 15:30.
- For example if you have a schedule where "evening" starts at 15:00 and the current time is 15:15
- If you create a schedule, when you exit scheduling the 119 will display the correct icon (morning, day,
evening, night) upon exiting. - You can erase scheduling by going into setup and modifying Option 9.
Remote Sensor
- Terminals S1 and S2 measure 3.3 vdc open.
- If the resistance is above 33 k, 32 flashes on the display.
- If the resistance is above 80k, OP is displayed and Off flashes.
- If the resistance is below 6k, 99 flashes on the display.
- If the resistance is below 1k, for some reason the 119 will enter Temporary Override on its own.
Below is a temperature / voltage chart.
BAYSENS119 Temperature / Voltage Chart
| Temp F | Temp C | DC Volts | Temp F | Temp C | DC Volts | Temp F | Temp C | DC Volts | ||
|---|---|---|---|---|---|---|---|---|---|---|
| 32 | 0.0 | 2.52 | 54 | 12.2 | 2.12 | 76 | 24.4 | 1.67 | ||
| 34 | 1.1 | 2.5 | 56 | 13.3 | 2.08 | 78 | 25.6 | 1.63 | ||
| 36 | 2.2 | 2.48 | 58 | 14.4 | 2.04 | 80 | 26.7 | 1.59 | ||
| 38 | 3.3 | 2.42 | 60 | 15.6 | 2 | 82 | 27.8 | 1.55 | ||
| 40 | 4.4 | 2.395 | 62 | 16.7 | 1.96 | 84 | 28.9 | 1.51 | ||
| 42 | 5.6 | 2.359 | 64 | 17.8 | 1.92 | 86 | 30.0 | 1.47 | ||
| 44 | 6.7 | 2.32 | 66 | 18.9 | 1.877 | 88 | 31.1 | 1.43 | ||
| 46 | 7.8 | 2.28 | 68 | 20.0 | 1.83 | 90 | 32.2 | 1.4 | ||
| 48 | 8.9 | 2.24 | 70 | 21.1 | 1.8 | 92 | 33.3 | 1.36 | ||
| 50 | 10.0 | 2.2 | 72 | 22.2 | 1.76 | 94 | 34.4 | 1.32 | ||
| 52 | 11.1 | 2.17 | 74 | 23.3 | 1.713 | 96 | 35.6 | 1.288 |
Zone Sensor Averaging
- In some applications 1 remote sensor does not give a good representation of the zone temperature.
- The quantity must be a "squared" number that allows them to be wired in series-parallel configuration.
- The resistance of the averaging circuit must duplicate the resistance of a single sensor.
- The quantities in the averaging circuit will be 4, 9, 16 or etc.
- The fewest number of sensors required to accomplish space temperature averaging is four.
- A programmable sensor can not be used as one of the averaging sensors.
- Remote sensor wiring must be twisted / shielded, connect the shield to terminal 11.
- Space temperature averaging is accomplished by wiring the correct number of sensors as shown below.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.