The BAYSENS119* has the same programming options and capabilities as the BAYSENS019* but also has improved thermistors that increase sensing accuracy and are still compatible with all equipment using ReliaTel™ micro controls.
The BAYSENS119* can be used with VAV, constant volume, or heat pump equipment. Not compatible with BAS integration application. (Standalone control only)
Display all the symbols showing
| Error codes | ||
|---|---|---|
| E1 | Heat failure | Indicates that there is an error in the heating system. |
| E2 | Cool failure | Indicates that there is an error in the cooling system. |
| E3 | Test mode | Indicates that the system is operating in test mode. |
| E4 | Fan failure | Indicates that a fan failure has occurred and service is required. |
|
Notes: 1. On the display, error codes toggle with the clock. | ||
Please refer to the latest available literature when available. - Click the link below:
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.