Odyssey - Application Guide
Click the e-library symbol for the latest version
Or download at the end of the warning sign.
Introduction
The Symbio™ 700 installed on Odyssey split systems is a factory-installed and programmed controller, providing digital control and protection of the equipment.
The Symbio 700 has two model options:
- Standard Controller (Basic) — provides standard troubleshooting via on-board user interface (UI) and access to the Symbio Service and Installation mobile app
- Advanced Controller — introduces additional troubleshooting tools and Building Automation System interface via BACnet® (ANSI/ASHRAE Standard 135-2016), Modbus™, or LonTalk®. Also allows TGP2 and up to eight additional I/O via XM30 or XM32 expansion modules.
The Symbio 700 offers multiple equipment configuration options regardless of controller model. The Odyssey split system can be configured as the following system types:
- Conventional Thermostat Control (T-Stat)
- Space Temperature Control Constant Volume (CVZT) - Single or Dual Setpoint Zone Sensor
- Space Temperature Control Single Zone Variable Air Volume (VVZT) - Single or Dual Setpoint Zone Sensor
These configurations can be used with standard cooling or heat pump systems.
This guide provides information about the configuration, control capabilities, and troubleshooting of the Odyssey system with the Symbio 700 controller.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.